This amplifier reference design measures impressively well. I'm impressed, but have 2 questions. It drives approx. 80 Watts per channel into 4 Ohms at the threshold of clipping. The peak voltage at this threshold is approx. 25.3 Volts. Why was a 36 Volt PVD selected? Would the distortion be significantly higher with a PVDD at few Volts above the clipping threshold? Or, was the higher PVDD chosen so that the power supply could have less-precise regulation?
Also, why were 7uH amplifier output inductors chosen instead of the 15uH or 22uH values used in many of your eval boards? Does this particular design require less filtering for similarly low EMI?
Thanks,
Marty