Hello there,
we're currently evaluating the mentioned codec. Our use case is to read from a digital microphone and direct the output to a speaker. This function works perfectly on the TLV320DAC3203EVM, but our target hardware will have no MCLK to provide to the codec. So we're trying to configure the codec to use the internal clock (BCLK?) to drive the PLL and therefore the microphone and DAC - but we're struggling at this point, as we're only seeing an output of 1 Hz from the BCLK pin.
Could you help us setting up the correct registers, so the TLV320 can run "standalone", without MCLK?
Thanks in advance,
Philipp