This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

TPA2012D2: Input bias voltage in shut down mode

Prodigy 120 points

Replies: 1

Views: 113

Part Number: TPA2012D2

Hi all,

I have a quick question for TPA2012.

Input bias voltage of TPA2012 is 0V in shut down mode? (input bias circuit is not active in shut down mode?)

Best regards,

  • Hi, A. Sakai,

    During the shutdown mode, the channels are completely powered off, leaving only the BIAS Circuitry portion active to enable or disable the channels through the SDR and SDL pins. The rest of input and output voltages are powered off.

    Best regards,
    Luis Fernando Rodríguez S.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.