TAS2770 support team
TAS2770 supports battery voltage range between 4.5V and 16V as the datasheet mentioned. But the datasheet is not mentioned the audio performance when VBAT is dynamically variated. According to my estimation, the voltage fluctuation is approximately 1.7V at typical case. When VBAT variates 1.7V with 2.5A/us of slew rate due to the system heavy load, will the audio performance degrade? If YES, can you show the degradation quantitatively? And also, does the noise issue?
Regards,
Tamio