Output from lineLP to Lpga to earphone is ok, lineLP to Lpga to Ladc is ok, but from Dout to Ldac to earphone is silent,Din and Dout are connected
aic3101Write(0,0x02,0x44);
aic3101Write(0,0x03,0x91);/*pll enabled q=2,p=1*/
aic3101Write(0,0x04,0x20); /*j=8*/
aic3101Write(0,0x05,0x00);
aic3101Write(0,0x06,0x00);/*D*/
aic3101Write(0,0x0b,0x01);/*R=1*/
aic3101Write(0,0x65,0x01);/*CODEC_CLKIN uses CLKDIV_OUT*/
aic3101Write(0,0x08,0xD0);
aic3101Write(0,0x09,0x06);
aic3101Write(0,0x2a,0x94);
aic3101Write(0,0x19,0x00);
aic3101Write(0,0x13,0x06);
aic3101Write(0,0x18,0x00);
aic3101Write(0,0x16,0x04);
aic3101Write(0,0x0f,0x50);
aic3101Write(0,0x10,0x50);
aic3101Write(0,0x28,0x80);
aic3101Write(0,0x0e,0x88);
aic3101Write(0,0x07,0x0a);
aic3101Write(0,0x40,0x80);
aic3101Write(0,0x25,0xc0);
aic3101Write(0,0x26,0x06);
aic3101Write(0,0x2c,0x00);
aic3101Write(0,0x2b,0x00);
aic3101Write(0,0x41,0x79);
aic3101Write(0,0x33,0x79);
#if 1
aic3101Write(0,0x3f,0x80);/*PGA_R is routed to HPROUT.*/
aic3101Write(0,0x2e,0x80);/*PGA_L is routed to HPLOUT.*/
#endif