This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA2005D1: 4 ohm load

Part Number: TPA2005D1

Is the TPA2005D1  Capable of driving  4 ohm speaker with Vdd @ 5.0V. The datasheet implied  VDD should be  Maximum 4.2 V with 4 ohm load.

What performance would be compromised when using VDD @ 5V with 4 ohm load. 

  • Hi, Brooks,

    Yes, the TPA2005D1 can only handle 4ohms load with the voltage range of 2.5V to 4.2V. Having a higher power supply may result in a risk of overcurrent. Constant exposure levels beyond this range may damage the device. So, we don't recommend to use higher power supplies for this load.

    Best regards,
    Luis Fernando Rodríguez S.