Other Parts Discussed in Thread: OPA810
With the TINA model corrected, can also go on to test this 20Hz to 20kHz integrated input noise Vrms in this spec line, this also gives very close agreement to the this number indicating the model probably needs to be updated to 2.9nV flatband and 36nV at 100Hz (or 1.51kHz 1/f corner)
Just putting a sense voltage meter on the input node, gives these two "total noise" curves from 20Hz to 20kHz which is the integrated noise through 20kHz. The corrected model shows 0.504uVrms with the original model having too high 1/f corner (but too low of flatband value) shows about 0.6uVrms
The corrected model yields a 1.51kHz 1/f corner, putting that into this equation from my old noise app note gives an equivalent flat spot noise for integration purposes of 2.9nV*1.23 = 3.57nV, then taking that times root(20kHz-20Hz) gives an integrated Vrms = 0.506uVrms, closely matching the TINA sim number.
This is on page 7 of this app note,