Other Parts Discussed in Thread: PCM2902,
I would like to use the PCM2906C to accept two input channels and output 4 signals. My customer is reporting that the Behringer UCA202, based on the PCM2902, is able to offer a headphone jack that he believes is interfaced to the HID pins that allows the user to listen to both the input and output at the same time. I wanted to ask if that was possible on the PCM2906C using these pins, or how one might connect to the IC to accomplish this.
I believe the PCM2902 in the Behringer UCA202 supports this, and it seems to have a similar interface set so I was thinking it would be a similar configuration. I am also worried that's what is being reported to me is not accurate and the internals of that UCA202 are muxing signals together in a way I'm not aware of and not actually using the HID pins on the codec.