Other Parts Discussed in Thread: LMK04821
Hello,
I'm this guy: (please read that post first, conditions and LMK's configuration is the same of that post, we dind't change anything)

My problem is that back then we got both PLL1 and PLL2 locked, but now for some reason (we suspect thermally-related) PLL1 does no longer lock, while PLL2 locks. That happens in 4 prototype cards we have. They all locked, they no longer lock. That means that the LMK is getting input from the VCXO and we also checked that the 24.576 MHz reference still works. VCXO's Vtune sits about 100mV above midrail (1,75 V approx). Changing CP current to vary the loop bandwidth doesn't help.
As for diagnostics capabilities, in our PCB we have read access to Status_LD1 and Status_LD2 pins and read/write access to CLKin_SEL0 and SEL1. Clkin0 is being used in MOS mode for the 24 MHz reference while Clkin1 is exposed and we can inject some external signal through it if neccesary.
As stated in my previous post we identified that we had a design mistake with PLL1's loop filter component values and we haven't changed them, but with the mounted values the filter should still be more than reasonable enough to achieve lock according to simulations (Clock Design Tool).
Any clue about what might be happening?
Thanks in advance,
David