Part Number: LMK00308
Other Parts Discussed in Thread: , LMK00306EVM, LMK00306
Hello,
I have a question about LMK00308.
[Background #1]
The LVDS interface circuit with AC coupling to receiver with internal 100 ohm termination is listed in the datasheet as follows.
<D/S(snas576d) P.26 10.3.2 Termination for AC Coupled Differential Operation>
When driving a differential receiver with internal 100 Ω differential termination, a source termination resistor
should be placed before the AC coupling capacitors for proper DC biasing of the driver as shown in Figure 34.
[Background #2]
The following application is shown in scaa059c.
[Background #3]
By default, CLKoutB# is configured for LVDS output in LMK00308EVM.
This circuit is same as Figure 12 in scaa059c.
[Q]
Is source termination resigter really necessary when driving a differential receiver with internal 100 ohm differential termination?
Is CLKoutB# LVDS circuit in LMK00308EVM wrong ?
Best Regards,
Hiroshi Katsunaga