Part Number: LMX2492
Other Parts Discussed in Thread: LMX2594, CODELOADER, LMX2531
Can you please post the full TICS PRO source for the LMX2492? I have found the rampcalc.py file for the board, but I cannot find the device top-level python file. In this other forum you posted a zip with both a ramp and pll .py file for each of the devices. Can you please do the same for the LMX2492?
If it is not in the zip, is there another file that you can share to show the low level commands for reading and writing registers over USB? Is this a libusb sort of thing? I want to build my embedded device to 1) load in the hex output file from TICS PRO, because I have effectively defined the default settings using the GUI; 2) take API-like commands from python or similar to update a few key settings and automatically adjust the LMX registers to match. That way I can most leverage the GUI and only have to build controllers for a small number of features in the chip.
Thanks!
P.S. The TICS PRO gui is excellent. Much better than your competitor offerings and is a large part of why I'm going with the TI PLL. Great work. I love when you develop great tools to go along with your chips. Keep it up :]!!