This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK04828: Register read result right after register write

Guru 19785 points
Part Number: LMK04828


Hi Team,

Would there be a case that register read back value is not equal to the value which written just before ?

My customer is saying that, for example, when he wrote R0x106 = "0xF1", then read R0x106 right away, the returned value was "0x01".
After waiting some time and then read R0x106 again, it returned "0xF1".
Could this happen ? If it does,,,

  - Which register would show this symptom ?
  - How long does it take to reflect the register value ?

Thanks in advance

Best Regards,
Kawai

  • Hi Kawai,

    In general if the register itself is not a "readback" type, like setting N divider value, then user should be able to read back what they wrote right away. If it is a "readback" type of register such as lock status indicator then what is read back is irrelevant to what was written. So in general we don't expect any delay between reading and writing for non-readback type registers.

    In the example you mentioned, there are two variables, one is "wait some time" and the other is "write again". So I'm not sure which one is the dominant factor.  Is it that you have to read twice to get the right answer or is it that you have to wait for some time before attempting to read.

    Instead of reading a single register, try "read all registers" and / or type the register field name here and hit "read". It may be just a GUI problem.

    Regards,
    Hao

  • Hi Hao-san,

    I tried with the LMK04826EVM which obtained. However, I couldn't reproduce the issue which customer reported.

    The wrote value was read at the next readback. (read within 1 second)

     

    >In the example you mentioned, there are two variables, one is "wait some time" and the other is "write again". So I'm not sure which one is the dominant factor.  Is it that you have to read twice to get the right answer or is it that you have to wait for some time before attempting to read.

    Customer is testing with their own board with their tool and they say that if they "wait some time then readback" or "read twice", they could read the correct value which wrote.

    I am asking for further information.

    Best Regards,

    Kawai

  • Hi Kawai,

    There is a state machine inside the IC which controls the logic for powerdowns and other settings. While there are a few features (such as global IC powerdown/reset) which are implemented asynchronously, most functions in this state machine are clocked, and the clock is usually derived from the reference clock input. It may take a few clock cycles for the system to assert conditions in updated registers. In the example you gave, R0x106 upper nibble controls some CLKout0 powerdown bits. It is possible that the state machine clock is slow enough with respect to the SPI clock that immediate readback can poll the register values before they have completely changed.

    In general, we do not specify the write delay for these operations to complete, since these delays can change based on reference clock speed and are often affected by other register settings (e.g. a powerdown may be faster if some sub-blocks are already powered down). If precise delay information is required for a specific case, the delay can be measured accurately using the chip select (CS) pin signal. For example, with powerdowns:

    1. Insert a sense resistor on the relevant power rail (for R0x106, Vcc12_CG0) and probe the real-time differential voltage across this resistor
    2. Probe the CS line in the SPI bus
    3. Probe the reference clock
    4. Check the delay between communication complete and change in supply current, and quantify in reference clock cycles
    5. Repeat measurement several times to ensure consistency

    This method works well for register updates that yield measurable changes in output frequency, power consumption, etc.

    On the other hand, if all the customer needs is to guarantee the write has completed, they can continue to poll the register until the values read match the values written. This should work for any register that is not self-clearing (such as software reset).

    So to summarize:

    • Some register operations are tied to the state machine clock. If the state machine clock is slow compared to the communication speed, sometimes the old value can be read back before the new value is updated.
    • Precise timings for specific scenarios could be measured using the CS pin signal and looking for the expected external change (current consumption, frequency adjustment, etc)
    • Reading back the values until they match the written values is straightforward for any register that is not self-clearing. Self-clearing registers like the software reset register may need other methods like the one outlined above with the CS pin signal.

    Regards,