Other Parts Discussed in Thread: SN74AUP1G17, SN74AUP1G74
Hi team,
Do we have frequency divider 30Hz input, and 15Hz output with 1.8V?
Thanks.

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: SN74AUP1G17, SN74AUP1G74
Hi team,
Do we have frequency divider 30Hz input, and 15Hz output with 1.8V?
Thanks.

Hello,
This is a common application of the D-type flip-flop. Your signal is very slow -- is it a digital signal with fast transitioning edges (~ 10ns)?
I'd recommend to use the SN74AUP1G74 for a 1.8V signal -- if the inputs are slow transitioning, add a series Schmitt-trigger buffer to the input signal such as SN74AUP1G17.

The PRE\ and CLR\ pins should be terminated to VCC directly, despite my drawing showing them disconnected.
Hi Emrys,
Do you mean use SN74AUP1G74 + SN74AUP1G17?
Do we have any automotive grade device for this?
Thanks.
I would recommend selecting devices based on your application from our parametric search tools. We have many D-type flip-flops as well as Schmitt-trigger buffers in our portfolio.