This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCI6214: Fall-back

Part Number: CDCI6214


Hi,TI

Will the CDCI6214 chip have output in the fall-back mode?If there is an output, is the output four-way 156.25MHz?

  • Hello Dominic,

    I believe the chip is pre-configured for 156.25MHz four-way output, with 25MHz input selected by pin state (after power-up), and it looks like it will have outputs in fall-back mode. This is based on the fall-back mode register settings in TICS Pro.

    Regards,

    Derek Payne