Hi team,
- Could you tell the definition of I_EE and I_CC?
- Does the value of I_CC include the value of I_EE?
Customer wants to understand total current that is used in the IC.
Regards,
Noriyuki Takahashi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
- Could you tell the definition of I_EE and I_CC?
- Does the value of I_CC include the value of I_EE?
Customer wants to understand total current that is used in the IC.
Regards,
Noriyuki Takahashi
Hello Takahashi-san,
Regards,
Derek Payne
Derek
Thanks!
Customer wants to understand the maximum output current per each channel.
At 125 degreeC, the datasheet specifies as below.
IEE: 85mA max
ICC: 405mA max
So, in this case, is it OK that the maximum output current per channel are specified as below?
the maximum output current per channel = (405mA - 85mA)/10ch = about 32mA?
Regards,
Noriyuki Takahashi
Derek,
They have one more question.
The ambient temperature is 85 degree C. They would like to estimate the maximum output current per channel roughly.
To do that, they want to understand what brings the difference the max ICC = 405mA at 125 degree C and the max ICC = 385mA at 25, -55 degree C. Could you give any suggestion to estimate it?
Do you think they can use 405mA at 85 degree C?
Regards,
Noriyuki Takahashi
Takahashi-san,
about 32mA/CH -> I think this makes sense, yes
I suspect the difference between 25°C and 125°C for ICC comes from the voltage bias changing at the output of the PECL/ECL structure. the 2mA difference per output channel corresponds to about 100mV shift in output common mode voltage at the output pins. The difference will grow larger as temperature increases, so 85°C 405mA is a safe estimate of total current consumption.
Regards,
Derek Payne