Part Number: LMX2594
Hello,
Our customer need to confirm if two LMX2594 could output sweep signal which constant frequency difference is 10Mhz.
Best regards
Kailyn
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LMX2594
Hello,
Our customer need to confirm if two LMX2594 could output sweep signal which constant frequency difference is 10Mhz.
Best regards
Kailyn
Hello Kailyn,
LMX2594 can perform frequency sweep using the ramp functionality. I believe that in manual mode, if VCO calibration can be avoided, it will definitely be possible to maintain a constant frequency difference of 10MHz in the outputs at every ramp step. The frequency difference will vary during the switching portion of the ramp, and if VCO calibration must occur then there are no guarantees that the calibration will complete in the same amount of time for both devices.
In automatic ramping mode, it should also be possible to schedule the ramp behavior based on some number of phase detector cycles. The same description of exceptions and edge cases (during switching and calibration) applies here as well.
Regards,
Derek Payne