Part Number: LMK03328
Other Parts Discussed in Thread: CDCEL824, , LMK5B12204
Hi,
Can someone please suggest me a 4 channel output clock generator similar to LMK03328RHST
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Shifali,
LMK03328 has two high-frequency PLLs and good jitter performance. We don't have that many similar parts, especially not with reduced output count. The LMK5B12204 is the closest high-performance device I can think of with four outputs, and can be operated without using the on-board DPLL, but the frequency range of the first PLL is restricted to integer divides of 2500MHz ±100ppm. We do have a lower performance CDCEL824 with two PLLs and four outputs as well, but this may not be adequate jitter or maximum frequency for your system and is restricted to only LVCMOS outputs.
Regards,
Derek Payne