Other Parts Discussed in Thread: LMK04828, ADC12DJ5200RF, , USB2ANY
Hi,
I'm using two LMX2594 devices with 2 ADC12DJ5200RF ADCs. The input reference for both LMX2594 is buffered input from OSCout of LMK04828.
RFoutB is used as SYSREF output. SYNC pin has CMOS input from one of the SDCLKout of LMK04828. (Differential to single ended buffer used).
With VCO_PHASE_SYNC_EN = 1, there's no JESD output. Making this 0 and setting MASH_SEED value to a desired number I'm able to shift the output and get phase matched output. But this is frequency specific. As the frequency changes, phase matching is lost.
I want to phase match between the two LMX2594 devices independent of frequency. How do I proceed?