Other Parts Discussed in Thread: CDCI6214
Sorry, there's company LO on it
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: CDCI6214
Sorry, there's company LO on it
Hi Dominic,
Most of the register programming appears to be correct. I think your frequency error is a result of the crystal driver not being properly tuned for your crystal. I am looping in a colleague with greater part-specific knowledge for CDCI6214 to answer your questions.
Regards,
Derek Payne
Hi Dominic,
Can you check if PLL is locked first? You can do this in Ticspro. Read back all registers then check the value of register LOCK_DET.

If it doesn't lock, do below
1. Click "RECAL" 2. see if this turns into green "locked". 3. Now measure the frequency again.

Let's first make sure that the PLL is locked before moving into the crystal load cap direction.
Regards,
Hao
Hi Li,
Can you then try changing the internal load capacitance? In general the load capacitance shouldn't cause frequency variation of as much as 2MHz but just try it first. Reduce the load capacitance here and see if the frequency goes up. Also, what's your load capacitance on the board?

If this doesn't help then check the output termination and try measuring it with an Oscilloscope or another frequency counter. Always double check the lock status.
Regards,
Hao
Hi Hao,
Thank you for your reply!
I tried to change the internal capacitance to 3pf,but the the output frequency does not change,and no matter the load capacitance on the board is 3pf or 12pF the the output frequency does not change too.
The PLL is locked
Regards,
li
Hi Li,
Are you using XTAL or external reference clock? If you're using 25 MHz XTAL, then you should be able to use the fall back default configuration.
Regardless, can you enable Y0 and measure the clock frequency from Y0? Y0 is the buffered output of the reference clock. So if Y0 is not accurate, then it means that the problem is with the reference clock.
Regards,
Hao
Hi Li,
This can't be true. Are you using a frequency counter to accurately measure the frequency? Can you send me the Ticspro configuration you are using (In Ticspro, File -> Save)? Since you are using 25MHz XTAL, fall-back default should work for you.
Regards,
Hao
Hi Li,
A few things:
1. According to the schematic, the fall back default should give your some valid outputs. Check again if PLL is locked after toggling the "recal" bit. If unlocked, enable Y0 and see if there's any clock output from Y0.
2. For the previous configuration where you saw 2 MHz frequency error, measure the frequency with a frequency counter. If the error is still there, send me that configuration file.
Regards,
Hao