Part Number: LMK04832-SP
Hi experts
Is it possible/allowed to have activity on the SPI interface signals while the device is unpowered?
This is frequently desirable in 'cold sparing' applications with redundant components.
Thanks!
Jim B
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LMK04832-SP
Hi experts
Is it possible/allowed to have activity on the SPI interface signals while the device is unpowered?
This is frequently desirable in 'cold sparing' applications with redundant components.
Thanks!
Jim B
Hello Jim,
By un-powered, I presume you mean no supply voltage present vs. a POWERDOWN state. In this case we technically spec an abs max of Vcc + 0.3 V. So strictly speaking this is not allowed and violating this would result in large currents due to ESD diode conduction. But it is possible...
Both of the above items may be addressable by placing a series resistor at the input of the LMK04832-SP SPI lines and using less than 3.3-V LVCMOS. This may be acceptable but I couldn't assure this without going through the process to add to the datasheet.
If they program the device to POWERDOWN=1 the current consumption is max 5 mA... this may be less current into the device than through the ESD diodes (when high). Would this be an option?
73,
Timothy
Thanks Timothy
To comply with the datasheet I'll state that it doesn't support cold sparing with the power supply at 0V.
I will recommend keeping the device powered but setting POWERDOWN=1.
Best regards,
Jim B
Ok great. We'll take an action to look to see if there is anything that can be added to clarify other possible options.