Hi,
in the datasheet it is written that the MUXOUT pin is only in tri-state when CE is low. Is this the only way to set MUXOUT to tri-state?
If so, what is the best way to use two LMX2820 on the same SPI bus? Is it possible, in this scenario with a shared SPI bus, to read out registers via SPI from one PLL without having to disable the second PLL (via CE)?
Best regards
Joachim