Part Number: LMK03806
Other Parts Discussed in Thread: USB2ANY
hi,
i'm using an LMK03806BISQ on a custom board.
the OSCIN is a 10 MHz TCXO (single ended).
i use an FPGA board to manage the uWire link.
After some debug, i'm pretty sure that the link is correct,
using the readback to be sure that the registers are correctly programmed.
I need 12x10 MHz outputs (clkout0 to clkout11).
but my output frequency is equal to 11.4643 MHz instead of 10 MHz
i get 10 MHz only on oscout0, so i think that my 10 MHz TCXO is ok.
i don't get
R0 (INIT) 0x80020140 R0 0x00001D40 R1 0x00001D41 R2 0x00001D42 R3 0x00001D43 R4 0x00001D44 R5 0x00001D45 R6 0x11110006 R7 0x11110007 R8 0x11110008 R9 0x55555549 R10 0xD1C2400A R11 0x37F1100B R12 0x030C006C R13 0x3B03826D R14 0x0300000E R16 0xC1550410 R24 0x00000018 R26 0xAFA8001A R28 0x0010001C R29 0x0080019D R30 0x030004FE R31 0x001F001F
please, find attached the registers calculated with TICS pro
regards
C.ALEXANDRE