Part Number: LMK04828
Other Parts Discussed in Thread: LMK04832
Hi
I am using LMK04828 in Dual Loop Mode,
Input parameters :
Clk_in 1 : 200 MHz
Oscin : 122.88 MHz
Output parameters :
Dclkout0 : 400 MHz
Dclkout2 : 200 MHz
Sdclkout2 : 6.25 MHz
I need Zero Delay mode or Nested Zero Delay mode in my application.
It would be great if you help me with the configurations.