Part Number: LMK03328
I'm currently using the LMK03328 is my design. I've originally used TI's Webench in the past to come up with the output frequencies and settings. I need to change my output frequencies but have no clue on how to do. After trial and error I was able to get Clock Tree Architect to select the LMK03328. But all I get is a pdf file that tells me the area, current, jitter, power; however I get no info on what the reference oscillator, R divider, N divider, N Divider Fraction, or other critical detailed info should be. I've also tried using PLLatinum Sim which gets me closer however when I used a test frequency, parameter don't match what is in the PLL.tcs file which I know works. Plus, PLLatinum seems to show only one outputs and I have seven different outputs in my application. I've also tried using the Wizard in TICS Pro but that is really worthless as I'm not able to do anything. I've already spent a few hours trying to figure out how to use TI's tools. I suppose worse case I can just fiddle with all the selections until I get close to the output frequency I want but I assume that's not a very good method. Seems like this should be easier than this. In the old Webench I could have done all this within minutes. Am I missing something here?