Part Number: LMX2572
Other Parts Discussed in Thread: LMX2594
Dear,
I would need some further help regarding the phase shift option on the LMX2572, since I am not sure if this behaviour is normal.
I have two LMX2572 boards which are sweeping between 500 MHz and 2490 MHz, with a step of 10 MHz (200 number of steps). At each frequency the boards are phase synchronised and then a phase shift for 400 steps is performed (between 0.72-0.99 degree/step, depending on the frequency, since the resolution is changed with CHA_DIV). To validate the performance both signals are summed with a RF combiner and measured is the average amplitude. The signal output is shown in the figure below:

Since the cable length of the two outputs is different, the magnitude minimum should slowly shift up with the frequency. This almost matches the expectations, but there are also two unexpected behaviours:
1. At frequency f17 and f18 the minimum doesn't follow the order which means that the phase sync was unsuccessful.
2. At some frequencies (specially between f111- f129) it looks like the frequency shift is not linear since the shape is not as expected (eg. f1)
I have repeated the measurements and the results are the same, so could this be a configuration problem or its a hardware limitation? Later I would like to set a specific phase shift for each frequency, where I then also expect that it will match the setup.
below is my a screnschot of my basic setup, from where I then just recalculate the needed values (N, CH_DIV, PFD_DEL, ...)
thank you and best regards