Part Number: CDCP1803
Hello Team,
My Customer is looking for the recommended max operating junction temperature for performance. Only ambient temperature for performance is on the datasheet is this the same?
Regards,
Renan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: CDCP1803
Hello Team,
My Customer is looking for the recommended max operating junction temperature for performance. Only ambient temperature for performance is on the datasheet is this the same?
Regards,
Renan
Hi Renan,
All the min. and max. data in Electrical Characteristic section were determined with throughout characterization at different lots and temperatures. Users will get the datasheet specified performance if they operate the device within datasheet specified conditions.
Hello Noel,
Good day and thank you for this response.
so it is safe to say that the max operating junction temperature for performance for this device is 125°C?
Regards,
Renan
Hi Renan
Yes. If the max. junction temperature required is violated, there is risk that the part will be damaged as well.