Hi,
Per datasheet & functional block diagram the output clock buffer is capable of accepting xtal input. Assuming if I need to drive single ended clock output Bank A, can I leave CLKoutA0*& CLKoutA1* unconnected?
Do advise if I'm looking at the correct device if i need a buffer which supports 25MHz xtal input/ 3.3V 25MHz buffer clock output with 1 to 4 port output. Thanks.
BR,
Leo