This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2594: Use of Pre and Post R divider with SYNC

Part Number: LMX2594

Are there any limitations on using the Pre and Post R dividers on OSCin as long as the OSCIn frequency is less than or equal to 100 MHz?  Does it have any effect on the SYNC category of the design?  For example, using a 100 MHz OSCIn frequency but then using the dividers to use 25 MHz as the Fpd and an output frequency of 3750 MHz (N of 75, divider is 4 since it's SYNC mode) am I still in Category 1 -- SYNC mode required but no pulse/software necessary?