Part Number: LMK05318B
Other Parts Discussed in Thread: LMK05318
Hi,
I wish to configure the EEPROM using "method #2"(direct writes). Meaning writing to SRAM byte by byte, program EEPROM and the configuration will be active on next POR.
I don't want to write directly to the registers space because it will effect immediately.
What is the relation between register number and SRAM address?
e.g. I wish to set R233 (PRIREF) to 0xAA. In which address does SRAM holds the value that will be program to EEPROM and loaded to R233 at next POR?
PS - Table 9.9 in DS specify the following address as "user programmable" 5,11,249,250,251,252 in TICS Pro SW the address are 10,11,249,250,251,252. Which one is correct?
BR,
Ofir.