Part Number: LMK04832EVM
Other Parts Discussed in Thread: LMK04832
Hi,
We were using the LMK04832EVM with a 100 MHz clkin1 input ,
replacing the original default configuration clkin1 122.88 MHz.
Once we changed frequency from 122.88 MHz to 100MHz, the status LD1 goes off.
Though we've tried set the CLKin1 frequency from 122.88 MHz to 100MHz in TICS pro (CLKinX Control page, PLL1 and 2 page and Clock Outputs page),
it still couldn't get the acurate output frequency and PLL Lock.
Is it possible to get the two different output frequency(100MHz and 122.88MHz) which both are syncornized to the input 100MHz?
Which registers need to be set in TICS Pro to get the above request?
Thank you !
Best regards,
Alan