Part Number: LMX2572LP
Other Parts Discussed in Thread: LMX2594,
I would like to configure the RFout to be transmitting for short intervals of time, ideally configured by an external input (e.g. SYNC pin?) or configured via register settings.
The sequence is as such:
1. Calibrate for frequency 1
2. Send for a pre-defined interval of time (e.g. 500ns)
3. Stop transmitting
4. Calibrate for frequency 2
5. Send for pre-defined interval of time
6. Stop transmitting
7. etc.
Is this possible, or will I basically require SPI communications at each step?