This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK04806: Inquriy about a clock generator recommendation

Guru 11050 points
Part Number: LMK04806
Other Parts Discussed in Thread: LMK04228, LMK03318, LMK04828, LMK04808

Hello,

My customer is looking for a clock generator to generate the following clocks.

    - Refclk : 30.72MHz

    - Outclk0 : 245.76MHz 1EA (LVPECL/LVDS/LVCMOS)

    - Outclk1 : 491.52MHz 2EA (LVPECL/LVDS)

    - Outclk2 : 245.76MHz 2EA (LVPECL/LVDS)

    - Outclk3 (Optional) : 122.88MHz 1EA (LVPECLE/LVDS)

Outclk 0~2 should be synchronized with refclk, but Outclk3 does not necessarily have to be synchronized.

The customer prefers to use one device, and for this, Outclk3 can be removed.

Could you please recommend a suitable clock generator?

Thank you.

JH