Part Number: LMX2594
Hi,
I am trying to generate a dual output LO at 5.36GHz using the LMX2594. I seem to be getting lots of 100MHz spurs away from the LO as well as the VCO output as shown in the attached photo. I have powered both outputs and have connected a 100MHz reference signal. As this is outside of the VCO core, I have selected VCO3 and enabled the channel divider (generating 10.72 GHz and then dividing by 2 to get 5.36GHz)
I believe this is likely a code issue; however, I have attempted to debug my code and cannot see any issues. Has any ever experienced this before or know any likely registers which could be causing this issue.
Thanks,
Louis