Part Number: LMK5B12204
Other Parts Discussed in Thread: LMK5C33216,
Hello TI,
snas810a specifies the Logic Output high voltage V_OH as 1.2 V min @ 1mA. VDD_DIG implies that this is a 3.3V nominal port, so in SPI mode, for example, SDO would normally be connected to an 3.3V nominal input requiring a 2V as a minimum input high voltage.
Can SDO drive an input requiring 2V minimum? If so, would it be possible to improve the Logic Output Characteristics specifications or provide relevant V vs. I characteristic charts, please?