This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2820: MUX_OUT_DOUBLER Issue in Fast VCO Mode

Part Number: LMX2820

Hi Team,

I am using the LMX2820 in Fast VCO Calibration, Full Assist mode. I can switch between 5650-11300 MHz without any problems, but when I turn on MUX_OUT_DOUBLER above 11300 MHz, the signal is distorted in some areas. If I activate and write the DBLR_CAL_EN bit in R0 where these distorted areas, it was fixed (FCAL_EN = 0). This causes the calibration time to be extended. What do I need to do for if i am using MUX_OUT_DOUBLER in Fast VCO Calibration mode without any distorted areas?

Best regards.