Part Number: CDCI6214
Hello.
I need to run the CDCI6214 as zerodely buffer.
The input is 100MHz, differential HCSL type connected to REF input.
The outpus shall be as following
- Y1, 100MHz HCSL type
- Y4, 100MHz HCSL type
The I2C interface of CDCI is connected to MCU so I can configure the registers after EEPROM is loaded. I'd like to modify the registers without EEPROM modification.
I need clarifications on how modify the registers:
1. Do I need to use EEPROM 1?
2. What shall be the modification values of the registers after loading from EEPROM to configure the CDCI as described above?
Regards