Part Number: LMX2571
Other Parts Discussed in Thread: CODELOADER
We are setting the LMX2571 synt. to toggle between 2 frequencies using the TrCtl pin.
Pls see the attached register setting that we are using.
More information:
- Routing both F1, F2 to OUTBUF_RX_EN (this is used as LO to a mixer)
- Using TrCtl to toggle between F1 and F2
- Register R0 is set to 0x002983 during initial and 0x000983 during normal operation.
The problem is that during toggle we see only F1 at the output and no output at all on F2.
Also we do not know how to active in the codeloader PLL F2
Register settings
| R60 | 0x3CA000 |
| R58 | 0x3A8C00 |
| R53 | 0x357806 |
| R47 | 0x2F6000 |
| R42 | 0x2A0210 |
| R41 | 0x290810 |
| R40 | 0x28101C |
| R39 | 0x2711FB |
| R35 | 0x230C80 |
| R34 | 0x221000 |
| R33 | 0x210000 |
| R32 | 0x200000 |
| R31 | 0x1F0000 |
| R30 | 0x1E0000 |
| R29 | 0x1D0000 |
| R28 | 0x1C0000 |
| R27 | 0x1B0000 |
| R26 | 0x1A0000 |
| R25 | 0x190000 |
| R24 | 0x18001F |
| R23 | 0x171F44 |
| R22 | 0x168184 |
| R21 | 0x150101 |
| R20 | 0x14401F |
| R19 | 0x131200 |
| R18 | 0x12D990 |
| R17 | 0x117A40 |
| R16 | 0x100000 |
| R15 | 0x0F0000 |
| R14 | 0x0E0000 |
| R13 | 0x0D0000 |
| R12 | 0x0C0000 |
| R11 | 0x0B0000 |
| R10 | 0x0A0000 |
| R9 | 0x090000 |
| R8 | 0x08001F |
| R7 | 0x071F44 |
| R6 | 0x068184 |
| R5 | 0x050101 |
| R4 | 0x04401B |
| R3 | 0x031200 |
| R2 | 0x025E10 |
| R1 | 0x017A5F |
| R0 | 0x000983 |