Hello,
I am using LMK05318B part on my designed board, and I use PRIREF_P as input now, XO_P and XO_N( Pin 31 and Pin 32) are pulled down by me.
Can I pull down the two Pin 31 and Pin 32 (XO_P and XO_N)? Please confirm
Best regards,
Robbie Ju
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I am using LMK05318B part on my designed board, and I use PRIREF_P as input now, XO_P and XO_N( Pin 31 and Pin 32) are pulled down by me.
Can I pull down the two Pin 31 and Pin 32 (XO_P and XO_N)? Please confirm
Best regards,
Robbie Ju
Hello Robbie,
No, XO input is required for APLL to function and device cannot output a proper clock without APLL calibrated and locked.
PriRef and SecRef are used for the DPLL, if DPLL function is not needed then no need for inputs there.
Regards,
Amin