Part Number: LMH1983
Hi,
Good day.
Our customer has a similar question about the dimension and distance between the mounting holes of the SD1983EVK. Thus, I have referred them to the original post. However, they say that the dimensions indicated in the photograph(115.1536mm and 110.0836mm) are clearly not the same as the dimensions for the board which they have at hand, which are approximately 112mm and 105.5mm, respectively, according to their direct measurement.
Can you please verify which is the correct information? Thank you.
Regards,
Cedrick