Part Number: LMK00301
Hi Team,
For differential CLK input slew rate measurement, customer wants to know how to measure the slew rate? Are the two measurement points are 20% and 80%?

Best,
Stanley
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LMK00301
Hi Team,
For differential CLK input slew rate measurement, customer wants to know how to measure the slew rate? Are the two measurement points are 20% and 80%?

Best,
Stanley
Hi Stanley,
The slew rate measurement can be done by following these steps:
1) Use an input source with a slew rate > 3V/ns
2) Use a scope set to gather the Rise/Fall time measurement with a threshold of 20 to 80%.
3) Calculate: slew rate = ((0.8 - 0.2)*VIN,amplitude) / tRISE
Regards,
Jennifer