Other Parts Discussed in Thread: LMX2594, LMX2820
Hi,
We are planning to use the PLL LMX2594 or LMX2820 for our comb generation application. Below is the frequency which we will be generating using PLL using 120MHz Centum OCXO or 100MHz Wenzel OCXO
Spot 1: 4680MHz
Spot 2: 5040MHz
Spot 3: 5400MHz
Request you to share the tested results of the following.
1. Phase noise plots from 100Hz offset to 10MHz offset for 5400MHz output ( For LMX2594 and LMX2820)
2. Spectrum plots with 1000MHz Span and RBW 5MHz for 5400MHz output, to check the SNR of the output
3. Frequency settling time while changing the frequency outputs of PLL from 4680 to 5400MHz vice versa
Regards,
INBAVANAN