Part Number: LMX2491
LMX2491 ramping 1500 to 1515.625MHz. Operation is zero-increment RAMP0 followed by RAMP1 as in datasheet page 32 example. Using 40MHz PLL reference, Multiplier x1, R Divider x1, We initially load all the registers and then use writes to R2 power-up/power-down to minimise power. Interestingly we do not seem to need any signal to kick off the ramp; it starts itself on power-up. On R2 = 0x01 (POWERUP), locks fine after about 70us. RAMP_CMP0 has been preset to 1505MHz (10485760 0xA00000, R60 = 0x00, R61 = 0x00, R62 = 0xA0 as per TICS-Pro) with CMP0RAMP brought out through TRIG1 (R36 = 0xB2, R64 = 0x02). TRIG1 goes high just 2us after lock initially goes low at the beginning of the ramp and stays high throughout ramp. Any ideas - cannot get ramp comparison to work, it just goes high at the very beginning of the ramp and stays high until the end and power-down?