Part Number: CDCS502
Hi Expert,
Is there any variation of output frequency that is due to IC performance? (if SSC is not used(+/-0%), and if the input clock is defined as having no variation)
If yes, Is it change by x1 or x4 setting?
Thanks
Muk
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: CDCS502
Hi Expert,
Is there any variation of output frequency that is due to IC performance? (if SSC is not used(+/-0%), and if the input clock is defined as having no variation)
If yes, Is it change by x1 or x4 setting?
Thanks
Muk
Hello Muk,
in x1 setting the device acts as buffer and follows the input frequency. In x4 mode the internal PLL multiplies the input by 4. The PLL is phase and frequency locked to the input.
Variations of center frequency are coming only from the input.
regards,
Julian