Other Parts Discussed in Thread: LMX2595
I want to use the LMX2595 in the "Full assist" mode, so that I haven't to do the VCO calibration every time. My plan was to program the the PLL with TICS Pro at the desired output frequency with the VCO calibration and afterwards read back the registers R110 - R112 (rb_VCO_SEL, rb_VCO_CAPCTRL, rb_VCO_DACISET), so that I can program the PLL with these values (VCO_SEL, VCO_DACISET, VCO_CAPCTRL) and bypass the VCO calibration.
I tried to readback the mentioned registers via the "Read Register" button in the "Raw Registers" tab in TICS Pro. But all data bits were set to '1', which doesn't make sense. I also tried the "Read All Registers" button, but the result was the same: All the data byte of the registers were set to '1'.
Do you have an idea what went wrong? Do I have to change the configuration of the Eval Board?
Kind regards
Christian