Part Number: LMX2572
Other Parts Discussed in Thread: DAC38RF80
I am using two LMX2572 in an application where they have a constant offset fout (5MHz). So for example, the first Synthesizer will generate an output of 100MHz, and the second synthesizer will generate 105MHz.
I need to generate these frequencies very quickly (using full assist VCO calibration), but I also need the phase offset between them such that when the signals are mixed together, they generate a constant phase offset (essentially time delay).
I don't really know what it means to "synchronize" synthesizers with different output frequencies. Ultimately, I am just after a constant phase offset between these 2 synthesizers, such that at a different RF out (e.g. 200MHz and 205MHz) yields the same phase offset as the first RF out (100MHz and 105MHz).
Does this make sense? Can I achieve what I'm after using the sync pin?