This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK03328:Regarding abnormal operation of the output port of LMK03328

Part Number: LMK03328

I am using your company's LMK03328.
Out6&7 isn't working properly.
Output of Out6 stops in the middle.
Out7 is in an unstable state where the output stops or outputs.
Observed with an oscilloscope, other Outs are operating normally.

Is there anything you can think of as a possible factor in this situation?
IC Revision Difference Will this happen?
Please check the attached configuration file that we are using.LMK00328.tcs

R0	0x0010
R1	0x010B
R2	0x0232
R3	0x0302
R4	0x0401
R8	0x0802
R9	0x0900
R10	0x0AAE
R11	0x0B00
R12	0x0CDF
R13	0x0D00
R14	0x0E00
R15	0x0F00
R16	0x1000
R17	0x1100
R18	0x1230
R19	0x1300
R20	0x14FF
R21	0x15FF
R22	0x16FF
R23	0x1702
R24	0x1800
R25	0x19F5
R27	0x1B58
R28	0x1C28
R29	0x1D00
R30	0x1E00
R31	0x1F20
R32	0x2020
R33	0x2118
R34	0x2278
R35	0x2320
R36	0x2418
R37	0x2510
R38	0x2618
R39	0x273C
R40	0x2818
R41	0x293C
R42	0x2A31
R43	0x2B3C
R44	0x2C13
R45	0x2D0A
R46	0x2E00
R47	0x2F00
R49	0x3100
R50	0x32CA
R51	0x3303
R52	0x3400
R53	0x3500
R54	0x3600
R55	0x3700
R56	0x3806
R57	0x3908
R58	0x3A00
R59	0x3B32
R60	0x3C00
R61	0x3D00
R62	0x3E00
R63	0x3F00
R64	0x4000
R65	0x4101
R66	0x420C
R67	0x4304
R68	0x4401
R69	0x4504
R70	0x4607
R71	0x470B
R72	0x4808
R73	0x4900
R74	0x4A36
R75	0x4B00
R76	0x4C00
R77	0x4D00
R78	0x4E00
R79	0x4F00
R80	0x5001
R81	0x510C
R82	0x5204
R83	0x5301
R84	0x5404
R85	0x5507
R86	0x5600
R88	0x5800
R89	0x59DE
R90	0x5A01
R91	0x5B18
R92	0x5C01
R93	0x5D4B
R94	0x5E01
R95	0x5F86
R96	0x6001
R97	0x61BE
R98	0x6201
R99	0x63FE
R100	0x6402
R101	0x6547
R102	0x6602
R103	0x679E
R104	0x6800
R105	0x6900
R117	0x7500
R118	0x7607
R119	0x7705
R120	0x7800
R131	0x8300
R132	0x8407
R133	0x8505
R134	0x8600

  • Hi Kakeru,

    Can you share your scope images of OUT6 and OUT7?

    Hi Hao,

    Please check their configuration file.

    Regards,

    Jennifer

  • Hi Jennifer,

    There is no out7 output waveform.

    The output waveform of out7 is as shown in the figure below.



    I've confirmed that my config file is okay.

    Can you also check if my config file is correct?

    When I set the Outputs Muxes setting of Out7 to PRIEF instead of PLL, the output became normal.

    Is it a clue to the cause of this time?

  • Hi Kakeru,

    Please check a few things:

    1. Is the PLL locked? With current configuration, PLL1 lock status can be read from pin STATUS1. LOL means Loss of Lock. So if STATUS1 pin is low, it means PLL1 is locked. If it's not locked, try doing a soft reset by toggling the RESETN_SW bit.

    2. If PLL is locked, try disabling the PLL1 output SYNC:

    3. Does this issue happen on all devices or just some devices? If it's the latter, did you do ABA swap to isolate the cause?

    Regards,
    Hao