Part Number: CDCLVP111-SP
Other Parts Discussed in Thread: CDCLVP111,
Following the datasheet of CDCLVP111, when utilizing an LVCMOS Oscillator we Bias the second input of CDCLVP111 to half the voltage of the Oscillator going into the primary input. Considering our Oscillator is powered at +2.5V and the biased voltage is +1.25V this would mean the input amplitude parameter for the datasheet below would be +1.25V correct?

If this is so then would it be correct in saying that this gives us a margin of 50mV from the max input amplitude?