Other Parts Discussed in Thread: REG101
Hi team,
One of our customers has the following questions. Can you provide ideas to solve the problems?

The reference signals of device 1 and device 2 come from the same clock. Sync is connected together. The same program is written to devices 1 and 2 through program control. Sync is controlled externally through pulse signal, and the output is not locked. When pulse is added, the frequency output is not coherent. Set bit 15 in register 58 to 0. When the external sync generates a pulse, the current will increase, but it is still not locked.
Best Regards,
Amy Luo