Part Number: CDCE6214-Q1
Hi,
My customer has the following questions. Could you please answer them?
On the CDCE6214-Q1 Register Map User's Guide (SNAU247B), Reserved bit is Zero on reset value. On the other hands, on the datasheet Table-22 "Register Defaults", Reserved bit also writes actual value. Which is default value? My understanding is "Register MAP User's guide is correct on reset value, but after de-asserted RESET, CDCE6214-Q1 update the value on the Table-22 of datasheet". Is it correct? Please advise us.
On "1.6.1 R60 Register" of CDCE6214-Q1 Register Map User's Guide (SNAU247B), CH1_CMOS_SLEW_RAT E_CTRL bit is 0x8 on RESET value, but "Do not use except 00h or 10h" on Description column. I think anything seems typo. I guess 0x8 is Normal mode. Could you please let us know what is correct?
On "7.21 Power-On Reset Characteristics" of datasheet, Start-up time is described on only Typical (9ms). Could you please let us know the MAX start-up time? Although this is not critical timing, he requires MAX value of start-up time for internal specification. Please advise us.
Thanks and best regards,
M.HATTORI.