Part Number: CDCE906
Other Parts Discussed in Thread: CDCE925
Hi,
I'm looking for a clockgenerator at 3.3V with the following:
- Clock input: CMOS 25MHz, external oscillator
- Outputs at 3.3V levels
- Output1: 48.000MHz
- Output2: 13.271MHz
- Output3: 25MHz with spreadspectrum
The datasheet is from year 2007, so I'm wondering if the CDCE906 is the best solution and how long this device will be in production.
Best regards,
Wim